Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static ImageBaseBuilder.InsertionPoint |
ImageBaseBuilder.InsertionPoint.DEFAULT
default insertion point type
|
static ImageBaseBuilder.InsertionPoint |
ImageBaseBuilder.InsertionPoint.USER_DEFINED
user defined insertion point type
|
Modifier and Type | Method and Description |
---|---|
ImageBaseBuilder.InsertionPoint |
ImageBaseBuilder.insertionPointOption()
Returns the image insertion point type
License requirements: None. |
static ImageBaseBuilder.InsertionPoint |
ImageBaseBuilder.InsertionPoint.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ImageBaseBuilder.InsertionPoint |
ImageBaseBuilder.InsertionPoint.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ImageBaseBuilder.InsertionPoint[] |
ImageBaseBuilder.InsertionPoint.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ImageBaseBuilder.setInsertionPointOption(ImageBaseBuilder.InsertionPoint insertPoint)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.