Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType.HIGH
static image output resolution of 300 DPI (dots per inch)
|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType.LOW
static image output resolution of 72 DPI (dots per inch)
|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType.MEDIUM
static image output resolution of 150 DPI (dots per inch)
|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType.USER_DEFINED
user specified image output resolution in DPI (dots per inch)
|
Modifier and Type | Method and Description |
---|---|
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
IRayPlusStudioEditorBuilder.irayPlusStudioStaticImageResolution()
Returns the Ray Traced Studio static image resolution
License requirements: studio_render ("UG STUDIO RENDER") . |
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType |
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType[] |
IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IRayPlusStudioEditorBuilder.setIRayPlusStudioStaticImageResolution(IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType iRayPlusStudioStaticImageResolution)
License requirements: studio_render ("UG STUDIO RENDER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.