Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Interface and Description |
---|---|
interface |
LightweightSection
Represents a PMI Lightweight Section
To create or edit an instance of this class, use LightweightSectionBuilder Created in NX7.5.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
BoundedGrid
Represents a bounded grid
Bounded grids are not supported in KF. |
interface |
DatumPlaneGrid
Represents a grid on a datum plane
Datum plane grids are not supported in KF. |
interface |
DynamicSection
Represents a dynamic section
To create or edit an instance of this class, use DynamicSectionBuilder Created in NX6.0.0 |
interface |
Grid
Represents a grid
Grids are not supported in KF. |
interface |
PlaneGrid
Represents a grid on a bounded plane
Plane grids are not supported in KF. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.