Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static FacetSettingsBuilder.FacetToViewRatio |
FacetSettingsBuilder.FacetToViewRatio.AUTOMATIC
Deprecated.
|
static FacetSettingsBuilder.FacetToViewRatio |
FacetSettingsBuilder.FacetToViewRatio.USER_DEFINED
Deprecated.
|
Modifier and Type | Method and Description |
---|---|
FacetSettingsBuilder.FacetToViewRatio |
FacetSettingsBuilder.advVisFacetToViewRatio()
Deprecated.
Deprecated in NX9.0.0. Refer to
FacetSettingsBuilder.advVisFacetScale() instead
|
FacetSettingsBuilder.FacetToViewRatio |
FacetSettingsBuilder.shadedFacetToViewRatio()
Deprecated.
Deprecated in NX9.0.0. Refer to
FacetSettingsBuilder.shadedFacetScale() instead
|
static FacetSettingsBuilder.FacetToViewRatio |
FacetSettingsBuilder.FacetToViewRatio.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static FacetSettingsBuilder.FacetToViewRatio |
FacetSettingsBuilder.FacetToViewRatio.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static FacetSettingsBuilder.FacetToViewRatio[] |
FacetSettingsBuilder.FacetToViewRatio.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FacetSettingsBuilder.setAdvVisFacetToViewRatio(FacetSettingsBuilder.FacetToViewRatio advVisFacetToViewRatio)
Deprecated.
Deprecated in NX9.0.0. Refer to
FacetSettingsBuilder.setAdvVisFacetScale(nxopen.display.FacetSettingsBuilder.FacetScale) instead
|
void |
FacetSettingsBuilder.setShadedFacetToViewRatio(FacetSettingsBuilder.FacetToViewRatio shadedFacetToViewRatio)
Deprecated.
Deprecated in NX9.0.0. Refer to
FacetSettingsBuilder.setShadedFacetScale(nxopen.display.FacetSettingsBuilder.FacetScale) instead
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.