Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static EnvironmentBuilder.ImageUpVectorTypes |
EnvironmentBuilder.ImageUpVectorTypes.ALIGN_WITH_FLOOR_PLANE |
static EnvironmentBuilder.ImageUpVectorTypes |
EnvironmentBuilder.ImageUpVectorTypes.USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
EnvironmentBuilder.ImageUpVectorTypes |
EnvironmentBuilder.imageUpVectorType()
Returns the image up vector define
License requirements: studio_render ("UG STUDIO RENDER") . |
static EnvironmentBuilder.ImageUpVectorTypes |
EnvironmentBuilder.ImageUpVectorTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EnvironmentBuilder.ImageUpVectorTypes |
EnvironmentBuilder.ImageUpVectorTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EnvironmentBuilder.ImageUpVectorTypes[] |
EnvironmentBuilder.ImageUpVectorTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EnvironmentBuilder.setImageUpVectorType(EnvironmentBuilder.ImageUpVectorTypes imageUpVector)
License requirements: studio_render ("UG STUDIO RENDER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.