Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static DynamicSectionTypes.Axis |
DynamicSectionTypes.Axis.NONE
Arbitrary axis
|
DynamicSectionTypes.Axis |
DynamicSectionBuilder.ActivePlaneData.planeaxis |
static DynamicSectionTypes.Axis |
DynamicSectionTypes.Axis.X
X axis
|
static DynamicSectionTypes.Axis |
DynamicSectionTypes.Axis.Y
Y axis
|
static DynamicSectionTypes.Axis |
DynamicSectionTypes.Axis.Z
Z axis
|
Modifier and Type | Method and Description |
---|---|
DynamicSectionTypes.Axis |
DynamicSectionBuilder.defaultPlaneAxis()
Returns the axis indicating the default plane normal.
|
static DynamicSectionTypes.Axis |
DynamicSectionTypes.Axis.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DynamicSectionTypes.Axis |
DynamicSectionTypes.Axis.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DynamicSectionTypes.Axis[] |
DynamicSectionTypes.Axis.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
DynamicSectionBuilder.PlaneGeometryData |
DynamicSectionBuilder.getPlaneGeometry(DynamicSectionTypes.Axis axisType,
DynamicSectionTypes.ActivePlane planeType)
Gets geometry of specified plane of the section.
|
double |
DynamicSectionBuilder.getRotationAngle(DynamicSectionTypes.Axis rotationAxis)
Gets rotation angle for specified axis.
|
void |
DynamicSectionBuilder.setActivePlane(DynamicSectionTypes.Axis planeAxis,
DynamicSectionTypes.ActivePlane activePlane)
|
void |
DynamicSectionBuilder.setDefaultPlaneAxis(DynamicSectionTypes.Axis planeAxis)
License requirements: None. |
void |
DynamicSectionBuilder.setRotationAngle(DynamicSectionTypes.Axis rotationAxis,
double angle)
Rotates the section about specified axis by the specified angle.
|
void |
DynamicSectionBuilder.setRotationMatrix(DynamicSectionTypes.Axis rotationAxis,
Matrix3x3 rotationMatrix)
Sets the section rotation matrix
Specify NONE
if the axis about which rotation was performed is not known. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.