Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Method and Description |
---|---|
DynamicSection |
ModelingView.activeDynamicSection()
Returns the active dynamic section object in the modeling view.
|
Modifier and Type | Method and Description |
---|---|
boolean |
ModelingView.isDynamicSectionVisible(DynamicSection dynamicSection)
Returns if the specified dynamic section object is visible
in this view.
|
void |
ModelingView.setActiveDynamicSection(DynamicSection dynamicSection)
License requirements: None. |
void |
ModelingView.setDynamicSectionVisible(DynamicSection dynamicSection,
boolean visible)
Sets the specified dynamic section object is visible/invisible
in this view.
|
Modifier and Type | Interface and Description |
---|---|
interface |
LightweightSection
Represents a PMI Lightweight Section
To create or edit an instance of this class, use LightweightSectionBuilder Created in NX7.5.0 |
Modifier and Type | Method and Description |
---|---|
DynamicSection[] |
DynamicSectionCollection.copySections(DynamicSection[] sections,
boolean deleteOriginals)
Copies the specified dynamic sections in the part.
|
DynamicSection |
DynamicSectionCollection.findObject(String journalIdentifier)
Finds the
DynamicSection with the given identifier as
recorded in a journal. |
Modifier and Type | Method and Description |
---|---|
DynamicSection[] |
DynamicSectionCollection.copySections(DynamicSection[] sections,
boolean deleteOriginals)
Copies the specified dynamic sections in the part.
|
DynamicSectionBuilder |
DynamicSectionCollection.createSectionBuilder(DynamicSection section,
ModelingView view)
Creates a
DynamicSectionBuilder object if the section
is null. |
void |
DynamicSectionCollection.deleteSections(boolean addUndoMark,
DynamicSection[] sections)
Deletes the specified dynamic sections in the part.
|
void |
DynamicSectionCollection.moveToDefaultLayer(DynamicSection[] dynamicSections)
Moves the specified dynamic sections in the part to default layer.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.