Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static CgfxMattexBuilder.UseCameraDirectionPlane |
CgfxMattexBuilder.UseCameraDirectionPlane.NORMAL_AND_UP_VECTOR
both normal and up vectors are updated based on camera direction
|
static CgfxMattexBuilder.UseCameraDirectionPlane |
CgfxMattexBuilder.UseCameraDirectionPlane.NORMAL_VECTOR
normal vector is updated based on camera direction
|
Modifier and Type | Method and Description |
---|---|
CgfxMattexBuilder.UseCameraDirectionPlane |
CgfxMattexBuilder.useCameraDirectionPlaneOption()
Deprecated.
Deprecated in NX10.0.0. No alternative provided for this class.
|
static CgfxMattexBuilder.UseCameraDirectionPlane |
CgfxMattexBuilder.UseCameraDirectionPlane.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CgfxMattexBuilder.UseCameraDirectionPlane |
CgfxMattexBuilder.UseCameraDirectionPlane.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CgfxMattexBuilder.UseCameraDirectionPlane[] |
CgfxMattexBuilder.UseCameraDirectionPlane.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CgfxMattexBuilder.setUseCameraDirectionPlaneOption(CgfxMattexBuilder.UseCameraDirectionPlane useCameraDiretionPlaneOption)
Deprecated.
Deprecated in NX10.0.0. No alternative provided for this class.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.