Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static CameraBuilder.Aperture |
CameraBuilder.Aperture.F11
f11
|
static CameraBuilder.Aperture |
CameraBuilder.Aperture.F16
f16
|
static CameraBuilder.Aperture |
CameraBuilder.Aperture.F22
f22
|
static CameraBuilder.Aperture |
CameraBuilder.Aperture.F28
f2.8
|
static CameraBuilder.Aperture |
CameraBuilder.Aperture.F56
f5.6
|
static CameraBuilder.Aperture |
CameraBuilder.Aperture.F8
f8
|
Modifier and Type | Method and Description |
---|---|
CameraBuilder.Aperture |
CameraBuilder.apertureType()
Returns the aperture
License requirements: None. |
static CameraBuilder.Aperture |
CameraBuilder.Aperture.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CameraBuilder.Aperture |
CameraBuilder.Aperture.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CameraBuilder.Aperture[] |
CameraBuilder.Aperture.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CameraBuilder.setApertureType(CameraBuilder.Aperture apertureType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.