public interface GridCollection extends TaggedObjectCollection
BasePart
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
DatumPlaneGridBuilder |
createDatumPlaneGridBuilder(DatumPlane[] datumPlanes)
Creates a
DatumPlaneGridBuilder object
used to build datum plane grids based on the supplied datum plane list. |
DatumPlaneGridBuilder |
createDatumPlaneGridBuilder(DatumPlaneGrid grid)
Creates a
DatumPlaneGridBuilder object
used to edit the supplied datum plane grid. |
PlanarShipGridBuilder |
createPlanarShipGridBuilder(PlanarShipGrid grid)
Creates a
PlanarShipGridBuilder object
used to build a planar ship grid on a datum plane. |
PlaneGridBuilder |
createPlaneGridBuilder(PlaneGrid grid)
Creates a
PlaneGridBuilder object
used to build a bounded grid on a plane. |
Grid |
findObject(String journalIdentifier)
Finds the
Grid with the given identifier
as recorded in a journal. |
DatumPlaneGrid |
getDatumPlaneGrid(DatumPlane datumPlane)
Finds the datum grid associated with the specified datum plane.
|
_find_next, iterator
PlaneGridBuilder createPlaneGridBuilder(PlaneGrid grid) throws NXException, RemoteException
PlaneGridBuilder
object
used to build a bounded grid on a plane.
If the grid is not null, the planar grid object will be edited.
grid
- If grid is not null,
then this object will be
editedNXException
RemoteException
DatumPlaneGridBuilder createDatumPlaneGridBuilder(DatumPlaneGrid grid) throws NXException, RemoteException
DatumPlaneGridBuilder
object
used to edit the supplied datum plane grid.
grid
- If grid is not null,
then this object will be
editedNXException
RemoteException
DatumPlaneGridBuilder createDatumPlaneGridBuilder(DatumPlane[] datumPlanes) throws NXException, RemoteException
DatumPlaneGridBuilder
object
used to build datum plane grids based on the supplied datum plane list.
datumPlanes
- datum plane listNXException
RemoteException
Grid findObject(String journalIdentifier) throws NXException, RemoteException
Grid
with the given identifier
as recorded in a journal. An object may not return the same value as
its JournalIdentifier in different versions of the software. However
newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In
general,this method should not be used in handwritten code and exists
to support record and playback of journals.
journalIdentifier
- Identifier to be foundNXException
RemoteException
DatumPlaneGrid getDatumPlaneGrid(DatumPlane datumPlane) throws NXException, RemoteException
datumPlane
- datum planeNXException
RemoteException
PlanarShipGridBuilder createPlanarShipGridBuilder(PlanarShipGrid grid) throws NXException, RemoteException
PlanarShipGridBuilder
object
used to build a planar ship grid on a datum plane.
If the grid is not null, the planar ship grid object will be edited.
grid
- If grid is not null,
this object will be editedNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.