Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Sketch.DimensionOption |
Sketch.DimensionOption.CREATE_AS_AUTOMATIC
Create dimension as automatic
|
static Sketch.DimensionOption |
Sketch.DimensionOption.CREATE_AS_DRIVING
Create dimension as driving
|
static Sketch.DimensionOption |
Sketch.DimensionOption.CREATE_AS_REFERENCE
Create dimension as reference
|
Modifier and Type | Method and Description |
---|---|
static Sketch.DimensionOption |
Sketch.DimensionOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.DimensionOption |
Sketch.DimensionOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.DimensionOption[] |
Sketch.DimensionOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
SketchDimensionalConstraint |
Sketch.createDiameterDimension(Sketch.DimensionGeometry dimObject1,
Point3d dimOrigin,
Expression expression,
Sketch.DimensionOption refDim)
Creates a diameter dimension constraint.
|
SketchDimensionalConstraint |
Sketch.createDimension(Sketch.ConstraintType dimType,
Sketch.DimensionGeometry dimObject1,
Sketch.DimensionGeometry dimObject2,
Point3d dimOrigin,
Expression expression,
Sketch.DimensionOption refDim)
Creates a dimension between two geometric objects.
|
SketchDimensionalConstraint |
Sketch.createRadialDimension(Sketch.DimensionGeometry dimObject1,
Point3d dimOrigin,
Expression expression,
Sketch.DimensionOption refDim)
Creates a radial dimension constraint.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.