Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Sketch.ConstraintPointType |
Sketch.ConstraintPointType.ANCHOR
The anchor point of a conic
|
static Sketch.ConstraintPointType |
Sketch.ConstraintPointType.ARC_CENTER
Center of a circle, arc, or ellipse
|
static Sketch.ConstraintPointType |
Sketch.ConstraintPointType.END_VERTEX
End vertex (e.g. the end point of a line)
|
static Sketch.ConstraintPointType |
Sketch.ConstraintPointType.MID_VERTEX
The mid vertex of a line or an arc
|
static Sketch.ConstraintPointType |
Sketch.ConstraintPointType.NONE
The geometry is not a point
|
Sketch.ConstraintPointType |
Sketch.ConstraintGeometry.pointType |
static Sketch.ConstraintPointType |
Sketch.ConstraintPointType.SPLINE_DEFINING_POINT
A defining point of a spline.
|
static Sketch.ConstraintPointType |
Sketch.ConstraintPointType.SPLINE_POLE
The control pole of a spline
|
static Sketch.ConstraintPointType |
Sketch.ConstraintPointType.START_VERTEX
Start vertex (e.g. the start point of a line)
|
Modifier and Type | Method and Description |
---|---|
static Sketch.ConstraintPointType |
Sketch.ConstraintPointType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.ConstraintPointType |
Sketch.ConstraintPointType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.ConstraintPointType[] |
Sketch.ConstraintPointType.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
ConstraintGeometry(NXObject geometryInitial,
Sketch.ConstraintPointType pointTypeInitial,
int splineDefiningPointIndexInitial)
Constructor for the ConstraintGeometry object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.