Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.fields |
Provides classes and interfaces for Fields.
|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
Modifier and Type | Method and Description |
---|---|
SelectObjectList |
SketchAutoConstrainBuilder.curveList()
Returns the selected curve list.
|
SelectObjectList |
GroupBuilder.objectsInGroup()
Returns the objects in group
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectObjectList |
QueryPmiBuilder.geometry()
Returns the geometry
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectObjectList |
ShowOnlyBuilder.selection()
Returns the selection
License requirements: None. |
SelectObjectList |
ShowHideBuilder.selection()
Returns the selection
License requirements: None. |
SelectObjectList |
ShowAdjacentBuilder.selection()
Returns the selection
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectObjectList |
UpdateViewsBuilder.views()
Returns the selected views
License requirements: drafting ("DRAFTING") . |
Modifier and Type | Method and Description |
---|---|
SelectObjectList |
ExtractFaceBuilder.bodyToExtract()
Deprecated.
Deprecated in NX9.0.0. Use
ExtractFaceBuilder.extractBodyCollector() instead.
|
SelectObjectList |
TrimSheetBuilder.boundaryObjects()
Returns the boundry objects
License requirements: None. |
SelectObjectList |
TrimCurveBuilder.curveList()
Returns the list of curves with the pick points
License requirements: None. |
SelectObjectList |
WaveDatumBuilder.datums()
Returns the datum to link
License requirements: None. |
SelectObjectList |
ProjectCurveBuilder.faceToProjectTo()
Returns the face to project to
License requirements: None. |
SelectObjectList |
TrimCurveBuilder.firstBoundingObject()
Returns the objects for the first boundary against which the selected curves are to be trimmed.
|
SelectObjectList |
IntersectionCurveBuilder.firstSet()
Returns the first set required only for non-associative intersection curve
License requirements: None. |
SelectObjectList |
GeomcopyBuilder.geometryToInstance()
Returns the selected object list of geometry to instance.
|
SelectObjectList |
SectionCurveBuilder.objectsToSection()
Returns the selected objects
License requirements: None. |
SelectObjectList |
TrimCurveBuilder.reverseTrimEnd()
Returns the curves the end to trim needs to be reversed
License requirements: None. |
SelectObjectList |
WaveRoutingBuilder.routingObjects()
Returns the routing
License requirements: None. |
SelectObjectList |
TrimCurveBuilder.secondBoundingObject()
Returns the objects for the second boundary against which the selected curves are to be trimmed.
|
SelectObjectList |
IntersectionCurveBuilder.secondSet()
Returns the second set required only for non-associative intersection curve
License requirements: None. |
SelectObjectList |
SectionCurveBuilder.sectionPlanes()
Returns the selected planes
License requirements: None. |
Modifier and Type | Interface and Description |
---|---|
interface |
PathObjects
Contains objects that define a lattice path
Not a KF builder; see Fields.FieldManager methods to create a Fields.PathObjects. |
Modifier and Type | Method and Description |
---|---|
SelectObjectList |
GeometricProperties.objectsForAnalysis()
Returns the Objects for analysis
License requirements: None. |
SelectObjectList |
ExamineGeometry.objectsToExamine()
Returns the Objects to examine
License requirements: None. |
SelectObjectList |
SolidDensity.solids()
Returns the solids to set density for
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.