Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Method and Description |
---|---|
SelectICurve |
SphereBuilder.arc()
Returns the selected arc associated with the Sphere.
|
SelectICurve |
CylinderBuilder.arc()
Returns the arc
License requirements: None. |
SelectICurve |
ConeBuilder.baseArc()
Returns the base arc
License requirements: None. |
SelectICurve |
DatumAxisBuilder.curve()
Returns the curve or edge.
|
SelectICurve |
AssociativeLineBuilder.endTangent()
Returns the end tangent - point can be passed in SELECT_OBJECT which is used in case of multiple solutions
License requirements: None. |
SelectICurve |
AssociativeLineBuilder.startTangent()
Returns the start tangent - point can be passed in SELECT_OBJECT which is used in case of multiple solutions
License requirements: None. |
SelectICurve |
ConeBuilder.topArc()
Returns the top arc
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.