Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static PositioningDimension.Subtype |
PositioningDimension.Subtype.ANGULAR
Angular dimension
|
static PositioningDimension.Subtype |
PositioningDimension.Subtype.HORIZONTAL
Horizontal dimension
|
static PositioningDimension.Subtype |
PositioningDimension.Subtype.LINE_ONTO_LINE
Line onto line dimension
|
static PositioningDimension.Subtype |
PositioningDimension.Subtype.PARALLEL
Parallel dimension
|
static PositioningDimension.Subtype |
PositioningDimension.Subtype.PARALLEL_DISTANCE
Parallel at a distance dimension
|
static PositioningDimension.Subtype |
PositioningDimension.Subtype.PERPENDICULAR
Perpendicular dimension
|
static PositioningDimension.Subtype |
PositioningDimension.Subtype.POINT_ONTO_LINE
Point onto line dimension
|
static PositioningDimension.Subtype |
PositioningDimension.Subtype.POINT_ONTO_POINT
Point onto point dimension
|
static PositioningDimension.Subtype |
PositioningDimension.Subtype.VERTICAL
Vertical dimension
|
Modifier and Type | Method and Description |
---|---|
PositioningDimension.Subtype |
PositioningDimension.getSubtype()
Returns the subtype of the dimension.
|
static PositioningDimension.Subtype |
PositioningDimension.Subtype.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PositioningDimension.Subtype |
PositioningDimension.Subtype.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PositioningDimension.Subtype[] |
PositioningDimension.Subtype.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
PositioningDimension.Subtype |
RPODimension.subtype()
Returns the subtype of the dimension.
|
Modifier and Type | Method and Description |
---|---|
void |
RPODimension.setSubtype(PositioningDimension.Subtype subtype)
License requirements: None. |
void |
RPOBuilder.setTargetAndTool(PositioningDimension.Subtype subtype,
NXObject target,
RPOBuilder.AssociativityType targetAssociativity,
Point3d targetHelpPoint,
NXObject tool,
RPOBuilder.AssociativityType toolAssociativity,
Point3d toolHelpPoint)
Sets the target and tool entities.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.