Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static PartCollection.MultipleDisplayedPartStatus |
PartCollection.MultipleDisplayedPartStatus.DISABLED
Indicates that only one part can be displayed at a time.
|
static PartCollection.MultipleDisplayedPartStatus |
PartCollection.MultipleDisplayedPartStatus.DISABLED_BY_CUSTOMER
Indicates that only one part can be displayed at a time.
|
static PartCollection.MultipleDisplayedPartStatus |
PartCollection.MultipleDisplayedPartStatus.ENABLED
It is possible to have more than one part be
displayed (i.e. additional different displayed parts).
|
Modifier and Type | Method and Description |
---|---|
PartCollection.MultipleDisplayedPartStatus |
PartCollection.allowMultipleDisplayedParts()
Returns the option indicating if more than one displayed part is allowed in this session.
|
static PartCollection.MultipleDisplayedPartStatus |
PartCollection.MultipleDisplayedPartStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartCollection.MultipleDisplayedPartStatus |
PartCollection.MultipleDisplayedPartStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartCollection.MultipleDisplayedPartStatus[] |
PartCollection.MultipleDisplayedPartStatus.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.