public static class PartCollection.MultipleDisplayedPartStatus extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DISABLED
Indicates that only one part can be displayed at a time.
|
static int |
_DISABLED_BY_CUSTOMER
Indicates that only one part can be displayed at a time.
|
static int |
_ENABLED
It is possible to have more than one part be
displayed (i.e. additional different displayed parts).
|
static PartCollection.MultipleDisplayedPartStatus |
DISABLED
Indicates that only one part can be displayed at a time.
|
static PartCollection.MultipleDisplayedPartStatus |
DISABLED_BY_CUSTOMER
Indicates that only one part can be displayed at a time.
|
static PartCollection.MultipleDisplayedPartStatus |
ENABLED
It is possible to have more than one part be
displayed (i.e. additional different displayed parts).
|
Modifier and Type | Method and Description |
---|---|
static PartCollection.MultipleDisplayedPartStatus |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartCollection.MultipleDisplayedPartStatus |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartCollection.MultipleDisplayedPartStatus[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartCollection.MultipleDisplayedPartStatus ENABLED
public static final PartCollection.MultipleDisplayedPartStatus DISABLED_BY_CUSTOMER
PartCollection.setAllowMultipleDisplayedParts(boolean)
rather than by the NX session itself.public static final PartCollection.MultipleDisplayedPartStatus DISABLED
public static final int _ENABLED
public static final int _DISABLED_BY_CUSTOMER
PartCollection.setAllowMultipleDisplayedParts(boolean)
rather than by the NX session itself.public static final int _DISABLED
public static PartCollection.MultipleDisplayedPartStatus valueOf(int value)
public static PartCollection.MultipleDisplayedPartStatus valueOf(String name)
public static PartCollection.MultipleDisplayedPartStatus[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.