Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MeshParameterData.FeatureType |
MeshParameterData.FeatureType.CURVE_MESH |
static MeshParameterData.FeatureType |
MeshParameterData.FeatureType.RULED |
static MeshParameterData.FeatureType |
MeshParameterData.FeatureType.THROUGH_CURVES |
Modifier and Type | Method and Description |
---|---|
static MeshParameterData.FeatureType |
MeshParameterData.FeatureType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeshParameterData.FeatureType |
MeshParameterData.FeatureType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeshParameterData.FeatureType[] |
MeshParameterData.FeatureType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
MeshParameterData.FeatureType |
MeshSurfaceBuilder.featureType()
Returns
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
Modifier and Type | Method and Description |
---|---|
void |
MeshSurfaceBuilder.buildProfileFromSections(boolean conehead,
MeshProfileString.Type profileStringType,
MeshParameterData.FeatureType skinType,
MeshProfileString.SelectedPoint stringPointType,
Section[] sections,
boolean editInsertProfile,
MeshProfileString profile)
Creates mesh surface profile string.
|
void |
MeshSurfaceBuilder.setFeatureType(MeshParameterData.FeatureType featureType)
Sets
License requirements: features_modeling ("FEATURES MODELING"), nx_freeform_1 ("basic freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.