Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static MeasureManager.ProjectionType |
MeasureManager.ProjectionType.MAX_CLEARANCE |
static MeasureManager.ProjectionType |
MeasureManager.ProjectionType.MAXIMUM |
static MeasureManager.ProjectionType |
MeasureManager.ProjectionType.MIN_CLEARANCE |
static MeasureManager.ProjectionType |
MeasureManager.ProjectionType.MINIMUM |
Modifier and Type | Method and Description |
---|---|
static MeasureManager.ProjectionType |
MeasureManager.ProjectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeasureManager.ProjectionType |
MeasureManager.ProjectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeasureManager.ProjectionType[] |
MeasureManager.ProjectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MeasureManager.editDistance(Measure feature,
DisplayableObject object1,
DisplayableObject object2,
Direction direction,
MeasureManager.ProjectionType projType)
Edit a projected minimum distance measure or clearance distance between two objects.Note that for design in
context the direction vector needs to be in the coordinates of the work part.
|
void |
MeasureManager.editDistance(String name,
DisplayableObject object1,
DisplayableObject object2,
Direction direction,
MeasureManager.ProjectionType projType)
Edit an embedded projected minimum or clearance distance measure between two objects.
|
MeasureDistance |
MeasureManager.newDistance(Unit units,
DisplayableObject object1,
DisplayableObject object2,
Direction direction,
MeasureManager.ProjectionType projType)
Create a projected, minimum clearance or maximum clearance distance measure between two objects.
|
MeasureDistance |
MeasureManager.newDistance(Unit units,
DisplayableObject object1,
DisplayableObject object2,
Direction direction,
MeasureManager.ProjectionType projType,
boolean createGeometry)
Create a projected, minimum clearance or maximum clearance distance measure between two objects with the
option to create smart geometry.
|
MeasureDistance |
MeasureManager.newScDistance(Unit units,
ScCollector collection1,
ScCollector collection2,
Direction direction,
MeasureManager.ProjectionType projType)
Create a projected, minimum clearance or maximum clearance distance measure between selection intent collections.
|
MeasureDistance |
MeasureManager.newScDistance(Unit units,
ScCollector collection1,
ScCollector collection2,
Direction direction,
MeasureManager.ProjectionType projType,
boolean createGeometry)
Create a projected, minimum clearance or maximum clearance distance measure between selection intent collections.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.