public static class MeasureManager.ProjectionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAX_CLEARANCE |
static int |
_MAXIMUM |
static int |
_MIN_CLEARANCE |
static int |
_MINIMUM |
static MeasureManager.ProjectionType |
MAX_CLEARANCE |
static MeasureManager.ProjectionType |
MAXIMUM |
static MeasureManager.ProjectionType |
MIN_CLEARANCE |
static MeasureManager.ProjectionType |
MINIMUM |
Modifier and Type | Method and Description |
---|---|
static MeasureManager.ProjectionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeasureManager.ProjectionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeasureManager.ProjectionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final MeasureManager.ProjectionType MINIMUM
public static final MeasureManager.ProjectionType MIN_CLEARANCE
public static final MeasureManager.ProjectionType MAX_CLEARANCE
public static final MeasureManager.ProjectionType MAXIMUM
public static final int _MINIMUM
public static final int _MIN_CLEARANCE
public static final int _MAX_CLEARANCE
public static final int _MAXIMUM
public static MeasureManager.ProjectionType valueOf(int value)
public static MeasureManager.ProjectionType valueOf(String name)
public static MeasureManager.ProjectionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.