Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Information.DisplayFeatureType |
Information.DisplayFeatureType.ALL
Displays all the information.
|
static Information.DisplayFeatureType |
Information.DisplayFeatureType.DEPENDENCIES
Displays dependencies information.
|
static Information.DisplayFeatureType |
Information.DisplayFeatureType.EXPRESSIONS
Displays expressions information.
|
static Information.DisplayFeatureType |
Information.DisplayFeatureType.FEATURES_IN_BODY
Displays features in body information.
|
static Information.DisplayFeatureType |
Information.DisplayFeatureType.PARAMETERS
Displays parameters information.
|
static Information.DisplayFeatureType |
Information.DisplayFeatureType.RELATED_OBJECT
Displays related(dual) object information.
|
Modifier and Type | Method and Description |
---|---|
static Information.DisplayFeatureType |
Information.DisplayFeatureType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Information.DisplayFeatureType |
Information.DisplayFeatureType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Information.DisplayFeatureType[] |
Information.DisplayFeatureType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Information.displayFeatureDetails(Feature feature,
Information.DisplayFeatureType type)
Displays relevant information about features created while
generating a 3-D model in the
ListingWindow . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.