public interface Information extends Remote
Session
Modifier and Type | Interface and Description |
---|---|
static class |
Information.DisplayFeatureType
Describes type of information displayed into listing window device.
|
Modifier and Type | Method and Description |
---|---|
void |
displayCamObjectsDetails(NXObject[] selectedObjects)
Display details of cam objects
License requirements: None. |
void |
displayFeatureDetails(Feature feature,
Information.DisplayFeatureType type)
Displays relevant information about features created while
generating a 3-D model in the
ListingWindow . |
void |
displayInterpartChildren(Part part)
Displays names of interpart children(part files having interlinked
geometry) in the
ListingWindow . |
void |
displayInterpartParents(Part part)
Displays names of interpart parents(part files having interlinked
geometry) in the
ListingWindow . |
void |
displayObjectsDetails(NXObject[] selectedObjects)
Displays information about geometric objects in the
ListingWindow . |
void |
displayPartHistory(BasePart part)
Displays the
ListingWindow with a part's save history. |
void |
displayPointDetails(Point point)
Obtains the absolute and work coordinates of an explicit or implicit point
and displays information in the
ListingWindow device. |
void |
displayPointDetails(Point3d absolutePointCoordinates)
Displays the absolute and work coordinates of a point
in the
ListingWindow device. |
void |
displayProdIntObjectsDetails(NXObject[] selectedObjects,
int startCounter)
Display details of product interface objects
License requirements: None. |
void |
displayUpdateStatusReport(Part part)
Displays status of all the features that failed to update
in the
ListingWindow . |
void displayPartHistory(BasePart part) throws NXException, RemoteException
ListingWindow
with a part's save history.
If we call this method externally without UI, it displays
the information on standard output device. The listing
window output can be sent to the Information window or to a
file, or to both. See ListingWindow.selectDevice(nxopen.ListingWindow.DeviceType, java.lang.String)
for more information.
part
- Part ObjectNXException
RemoteException
void displayPointDetails(Point point) throws NXException, RemoteException
ListingWindow
device.
If we call this method externally without UI, it displays
the information on standard output device. The listing
window output can be sent to the Information window or to a
file, or to both. See ListingWindow.selectDevice(nxopen.ListingWindow.DeviceType, java.lang.String)
for more information.
point
- Point ObjectNXException
RemoteException
void displayPointDetails(Point3d absolutePointCoordinates) throws NXException, RemoteException
ListingWindow
device.
If we call this method externally without UI, it displays
the information on standard output device. The listing
window output can be sent to the Information window or to a
file, or to both. See ListingWindow.selectDevice(nxopen.ListingWindow.DeviceType, java.lang.String)
for more information.
absolutePointCoordinates
- Absolute coordinates of a pointNXException
RemoteException
void displayObjectsDetails(NXObject[] selectedObjects) throws NXException, RemoteException
ListingWindow
.
If we call this method externally without UI, it displays
the information on standard output device. The listing
window output can be sent to the Information window or to a
file, or to both. See ListingWindow.selectDevice(nxopen.ListingWindow.DeviceType, java.lang.String)
for more information.
selectedObjects
- Array of objects for which the information is to be displayedNXException
RemoteException
void displayFeatureDetails(Feature feature, Information.DisplayFeatureType type) throws NXException, RemoteException
ListingWindow
.
If we call this method externally without UI, it displays
the information on standard output device. The listing
window output can be sent to the Information window or to a
file, or to both. See ListingWindow.selectDevice(nxopen.ListingWindow.DeviceType, java.lang.String)
for more information.
feature
- Feature objecttype
- Type of information to displayNXException
RemoteException
void displayInterpartChildren(Part part) throws NXException, RemoteException
ListingWindow
.
If we call this method externally without UI, it displays
the information on standard output device. The listing
window output can be sent to the Information window or to a
file, or to both. See ListingWindow.selectDevice(nxopen.ListingWindow.DeviceType, java.lang.String)
for more information.
part
- Part objectNXException
RemoteException
void displayInterpartParents(Part part) throws NXException, RemoteException
ListingWindow
.
If we call this method externally without UI, it displays
the information on standard output device. The listing
window output can be sent to the Information window or to a
file, or to both. See ListingWindow.selectDevice(nxopen.ListingWindow.DeviceType, java.lang.String)
for more information.
part
- Part objectNXException
RemoteException
void displayUpdateStatusReport(Part part) throws NXException, RemoteException
ListingWindow
.
If we call this method externally without UI, it displays
the information on standard output device. The listing
window output can be sent to the Information window or to a
file, or to both. See ListingWindow.selectDevice(nxopen.ListingWindow.DeviceType, java.lang.String)
for more information.
part
- Part objectNXException
RemoteException
void displayCamObjectsDetails(NXObject[] selectedObjects) throws NXException, RemoteException
selectedObjects
- Array of objects for which the information is to be displayedNXException
RemoteException
void displayProdIntObjectsDetails(NXObject[] selectedObjects, int startCounter) throws NXException, RemoteException
selectedObjects
- product interface objectsstartCounter
- start counter for object #NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.