Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CartesianCoordinateSystem
Represents a cartesian coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCoordinateSystem(nxopen.Point3d, nxopen.Matrix3x3, boolean) Created in NX4.0.0 |
interface |
CoordinateSystem
Represents a coordinate system
This is an abstract class . |
interface |
CylindricalCoordinateSystem
Represents a cylindrical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCylindricalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
interface |
DatumAxis
Represents a datum axis
This object can not be created by KF it's the display objet of the datum axis . |
interface |
Direction
Represents a direction.
|
interface |
Point
Represents a smart
Point . |
interface |
SphericalCoordinateSystem
Represents a spherical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createSphericalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
MeshPoint
Represents a smart
MeshPoint . |
Modifier and Type | Method and Description |
---|---|
ILocation |
PierceHoleChildBuilder.breakerHoleDirection()
Returns the breaker hole direction of the pierce hole
License requirements: ug_die_design ("Die Design") . |
ILocation |
PierceHoleChildBuilder.breakerHoleLocation()
Returns the location of breaker holes for the pierce hole
License requirements: ug_die_design ("Die Design") . |
ILocation |
TrimTaskBuilder.camDirection()
Returns the cam direction of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
ILocation |
PierceTaskBuilder.camDirection()
Returns the cam direction of the pierce task
License requirements: die_engineering ("DIE ENGINEERING") . |
ILocation |
FormTaskBuilder.camDirection()
Returns the cam direction of the form task.
|
ILocation |
FlangeTaskBuilder.camDirection()
Returns the cam direction of the flange task
License requirements: die_engineering ("DIE ENGINEERING") . |
ILocation |
HoleChildBuilder.center()
Returns the center of the die hole.
|
ILocation |
HandlingCoreChildBuilder.center()
Returns the center of the handling core.
|
ILocation[] |
PierceHoleChildBuilder.getPierceHoleLocation()
Gets the locations of the pierce hole
License requirements: ug_die_design ("Die Design") . |
ILocation |
PadChildBuilder.location()
Returns the location of the die pad.
|
ILocation |
PierceHoleChildBuilder.pierceHoleDirection()
Returns the pierce hole direction
License requirements: ug_die_design ("Die Design") . |
ILocation |
PierceItemBuilder.referenceVector()
Returns the reference direction of the hole
License requirements: die_engineering ("DIE ENGINEERING") . |
Modifier and Type | Method and Description |
---|---|
void |
PierceHoleChildBuilder.setBreakerHoleDirection(ILocation breakerHoleDirection)
Sets the breaker hole direction of the pierce hole
License requirements: ug_die_design ("Die Design") . |
void |
PierceHoleChildBuilder.setBreakerHoleLocation(ILocation breakerHoleLocation)
Sets the location of breaker holes for the pierce hole
License requirements: ug_die_design ("Die Design") . |
void |
TrimTaskBuilder.setCamDirection(ILocation camDirection)
Sets the cam direction of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
void |
PierceTaskBuilder.setCamDirection(ILocation camDirection)
Sets the cam direction of the pierce task
License requirements: die_engineering ("DIE ENGINEERING") . |
void |
FormTaskBuilder.setCamDirection(ILocation camDirection)
Sets the cam direction of the form task.
|
void |
FlangeTaskBuilder.setCamDirection(ILocation camDirection)
Sets the cam direction of the flange task
License requirements: die_engineering ("DIE ENGINEERING") . |
void |
HoleChildBuilder.setCenter(ILocation center)
Sets the center of the die hole.
|
void |
HandlingCoreChildBuilder.setCenter(ILocation center)
Sets the center of the handling core.
|
void |
PadChildBuilder.setLocation(ILocation location)
Sets the location of the die pad.
|
void |
PierceHoleChildBuilder.setPierceHoleDirection(ILocation pierceHoleDirection)
Sets the pierce hole direction
License requirements: ug_die_design ("Die Design") . |
void |
PierceHoleChildBuilder.setPierceHoleLocation(ILocation[] pierceHoleLocations)
Sets the locations of the pierce hole
License requirements: ug_die_design ("Die Design") . |
void |
PierceItemBuilder.setReferenceVector(ILocation refVector)
Sets the reference direction of the hole
License requirements: die_engineering ("DIE ENGINEERING") . |
Modifier and Type | Interface and Description |
---|---|
interface |
DraftingPoint
Represents a Drafting VD Point.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.