Package | Description |
---|---|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.gateway |
Provides classes and interfaces for Gateway.
|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
nxopen.pdm |
Provides classes and interfaces for PDM.
|
nxopen.pid |
Provides classes and interfaces for PID.
|
nxopen.plas |
Provides classes and interfaces for PLAS.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AddComponentBuilder
Represents a builder class that performs add existing component operation in current context.
|
interface |
CopyDesignElementBuilder
Represents a builder class that performs copying design element operation in 4GD.
|
interface |
DesignElementBuilder
Represents a builder class that performs various design element operations.
|
interface |
SubsetBuilder
A SubsetBuilder is used to create or edit an
Subset . |
Modifier and Type | Interface and Description |
---|---|
interface |
CopyPasteNewBuilder
Represents a
CopyPasteNewBuilder
It is used in Ship Building Application. |
Modifier and Type | Interface and Description |
---|---|
interface |
IGenericFileNewApplicationBuilder
Represents the class Application Builder.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AddSubmechanismBuilder
Represents a builder class that performs add submechanism in current context.
|
Modifier and Type | Interface and Description |
---|---|
interface |
ExportWorksetForReferenceBuilder
Represents a builder class that performs Create operations
To create a new instance of this class, use PdmSession.createExportWorksetForReferenceBuilder(nxopen.BasePart) Created in NX10.0.0 |
interface |
ObjectCreateBuilder
Represents a builder class that perofrms create operation
To create a new instance of this class, use PdmSession.createObjectCreateBuilder(java.lang.String[], java.lang.String[]) Created in NX10.0.0 |
interface |
PartOperationBuilder
Represents a builder class that performs various design element operations.
|
interface |
PartOperationCopyBuilder
Represents a builder class that performs various Save As operations.
|
interface |
PartOperationCreateBuilder
Represents a builder class that performs Create operations
To create a new instance of this class, use PdmSession.createCreateOperationBuilder(nxopen.pdm.PartOperationBuilder.OperationType) Created in NX10.0.0 |
interface |
PartOperationImportBuilder
Represents a builder class that performs Create operations
To create a new instance of this class, use PdmSession.createImportOperationBuilder() Default values. |
interface |
PartOperationMakeUniqueBuilder
Represents a
PartOperationMakeUniqueBuilder builder To create a new instance of this class, use PdmSession.createMakeUniqueOperationBuilder(nxopen.BasePart) Created in NX10.0.0 |
interface |
SmartSaveBuilder
TODO: Add a documentation comment describing this class.
|
Modifier and Type | Interface and Description |
---|---|
interface |
FileNewApplicationBuilder
Represents a builder class that performs Generic File New operations.
|
Modifier and Type | Interface and Description |
---|---|
interface |
RunBuilder
Represents a RunBuilder.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.