Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static ExtrudeOffsetDataOffsetType |
ExtrudeOffsetDataOffsetType.NONE
No offset
|
static ExtrudeOffsetDataOffsetType |
ExtrudeOffsetDataOffsetType.NORMAL_OFFSET
Offset with two different distances
|
static ExtrudeOffsetDataOffsetType |
ExtrudeOffsetDataOffsetType.SINGLE_OFFSET
Offset with single distance in one direction
|
static ExtrudeOffsetDataOffsetType |
ExtrudeOffsetDataOffsetType.SYMMETRIC_OFFSET
Offset with same distance in both directions
|
Modifier and Type | Method and Description |
---|---|
static ExtrudeOffsetDataOffsetType |
ExtrudeOffsetDataOffsetType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtrudeOffsetDataOffsetType |
ExtrudeOffsetDataOffsetType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtrudeOffsetDataOffsetType[] |
ExtrudeOffsetDataOffsetType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.