public class ExtrudeOffsetDataOffsetType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
No offset
|
static int |
_NORMAL_OFFSET
Offset with two different distances
|
static int |
_SINGLE_OFFSET
Offset with single distance in one direction
|
static int |
_SYMMETRIC_OFFSET
Offset with same distance in both directions
|
static ExtrudeOffsetDataOffsetType |
NONE
No offset
|
static ExtrudeOffsetDataOffsetType |
NORMAL_OFFSET
Offset with two different distances
|
static ExtrudeOffsetDataOffsetType |
SINGLE_OFFSET
Offset with single distance in one direction
|
static ExtrudeOffsetDataOffsetType |
SYMMETRIC_OFFSET
Offset with same distance in both directions
|
Modifier and Type | Method and Description |
---|---|
static ExtrudeOffsetDataOffsetType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtrudeOffsetDataOffsetType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtrudeOffsetDataOffsetType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ExtrudeOffsetDataOffsetType NONE
public static final ExtrudeOffsetDataOffsetType NORMAL_OFFSET
public static final ExtrudeOffsetDataOffsetType SYMMETRIC_OFFSET
public static final ExtrudeOffsetDataOffsetType SINGLE_OFFSET
public static final int _NONE
public static final int _NORMAL_OFFSET
public static final int _SYMMETRIC_OFFSET
public static final int _SINGLE_OFFSET
public static ExtrudeOffsetDataOffsetType valueOf(int value)
public static ExtrudeOffsetDataOffsetType valueOf(String name)
public static ExtrudeOffsetDataOffsetType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.