Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Axis.Types |
Axis.Types.NON_ASSOCIATIVE
non-associative
|
static Axis.Types |
Axis.Types.OTHER
the type is not one of the other enumerated types
|
static Axis.Types |
Axis.Types.POINT_AND_DIRECTION
the axis is defined by a
Point and AxisDirection |
Modifier and Type | Method and Description |
---|---|
Axis.Types |
Axis.type()
Returns the associativity type for the axis
License requirements: None. |
static Axis.Types |
Axis.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Axis.Types |
Axis.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Axis.Types[] |
Axis.Types.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.