public static class Axis.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NON_ASSOCIATIVE
non-associative
|
static int |
_OTHER
the type is not one of the other enumerated types
|
static int |
_POINT_AND_DIRECTION
the axis is defined by a
Point and AxisDirection |
static Axis.Types |
NON_ASSOCIATIVE
non-associative
|
static Axis.Types |
OTHER
the type is not one of the other enumerated types
|
static Axis.Types |
POINT_AND_DIRECTION
the axis is defined by a
Point and AxisDirection |
Modifier and Type | Method and Description |
---|---|
static Axis.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Axis.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Axis.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final Axis.Types NON_ASSOCIATIVE
public static final Axis.Types POINT_AND_DIRECTION
Point
and AxisDirection
public static final Axis.Types OTHER
public static final int _NON_ASSOCIATIVE
public static final int _POINT_AND_DIRECTION
Point
and AxisDirection
public static final int _OTHER
public static Axis.Types valueOf(int value)
public static Axis.Types valueOf(String name)
public static Axis.Types[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.