Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static WedmOperationBuilder.StopPointTypes |
WedmOperationBuilder.StopPointTypes.OPSTOP
stop point option opstop
|
static WedmOperationBuilder.StopPointTypes |
WedmOperationBuilder.StopPointTypes.STOP
stop point option stop
|
Modifier and Type | Method and Description |
---|---|
WedmOperationBuilder.StopPointTypes |
WedmOperationBuilder.stopPointType()
Returns the Stop Point Type
License requirements: cam_base ("CAM BASE") . |
static WedmOperationBuilder.StopPointTypes |
WedmOperationBuilder.StopPointTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WedmOperationBuilder.StopPointTypes |
WedmOperationBuilder.StopPointTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WedmOperationBuilder.StopPointTypes[] |
WedmOperationBuilder.StopPointTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WedmOperationBuilder.setStopPointType(WedmOperationBuilder.StopPointTypes stopPointType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.