Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static WedmGeomBuilder.SmoothLeadOutTypes |
WedmGeomBuilder.SmoothLeadOutTypes.NONE
smooth leadin type none
|
static WedmGeomBuilder.SmoothLeadOutTypes |
WedmGeomBuilder.SmoothLeadOutTypes.SPECIFY
smooth leadin type specify
|
Modifier and Type | Method and Description |
---|---|
WedmGeomBuilder.SmoothLeadOutTypes |
WedmGeomBuilder.smoothLeadOutOption()
Returns the Smooth Leadout Flag
License requirements: cam_base ("CAM BASE") . |
static WedmGeomBuilder.SmoothLeadOutTypes |
WedmGeomBuilder.SmoothLeadOutTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WedmGeomBuilder.SmoothLeadOutTypes |
WedmGeomBuilder.SmoothLeadOutTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WedmGeomBuilder.SmoothLeadOutTypes[] |
WedmGeomBuilder.SmoothLeadOutTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WedmGeomBuilder.setSmoothLeadOutOption(WedmGeomBuilder.SmoothLeadOutTypes leadOutOption)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.