Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static WedmCutParameters.WirePositionTypes |
WedmCutParameters.WirePositionTypes.ON
drive on
|
static WedmCutParameters.WirePositionTypes |
WedmCutParameters.WirePositionTypes.TANTO
drive tanto
|
Modifier and Type | Method and Description |
---|---|
static WedmCutParameters.WirePositionTypes |
WedmCutParameters.WirePositionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WedmCutParameters.WirePositionTypes |
WedmCutParameters.WirePositionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WedmCutParameters.WirePositionTypes[] |
WedmCutParameters.WirePositionTypes.values()
Returns an array that contains the values for this enum.
|
WedmCutParameters.WirePositionTypes |
WedmCutParameters.wirePosition()
Returns the wire position
License requirements: cam_base ("CAM BASE") . |
Modifier and Type | Method and Description |
---|---|
void |
WedmCutParameters.setWirePosition(WedmCutParameters.WirePositionTypes wirePosition)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.