Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
WedmCustomBoundaryDataBuilder |
WedmCustomBoundaryDataBuilderList.findItem(int index)
Returns the object at the input index.
|
WedmCustomBoundaryDataBuilder[] |
WedmCustomBoundaryDataBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
WedmCustomBoundaryDataBuilderList.append(WedmCustomBoundaryDataBuilder object)
Appends an object to the list
License requirements: None. |
void |
WedmCustomBoundaryDataBuilderList.append(WedmCustomBoundaryDataBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
WedmCustomBoundaryDataBuilderList.erase(WedmCustomBoundaryDataBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
WedmCustomBoundaryDataBuilderList.erase(WedmCustomBoundaryDataBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
WedmCustomBoundaryDataBuilderList.findIndex(WedmCustomBoundaryDataBuilder obj)
Finds the index where the input object appears.
|
void |
WedmCustomBoundaryDataBuilderList.insert(int location,
WedmCustomBoundaryDataBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
WedmCustomBoundaryDataBuilderList.setContents(WedmCustomBoundaryDataBuilder[] objects)
Sets the contents of the entire list.
|
void |
WedmCustomBoundaryDataBuilderList.swap(WedmCustomBoundaryDataBuilder object1,
WedmCustomBoundaryDataBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.