Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
WedmExtGeomBuilder
Represents a WedmExtGeom Builder
To create a new instance of this class, use NCGroupCollection.createWedmExtGeomBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
WedmFeatureGeomBuilder
Represents a WedmFeatureGeom Builder
To create a new instance of this class, use NCGroupCollection.createWedmFeatureGeomBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
WedmIntGeomBuilder
Represents a WedmIntGeom Builder
To create a new instance of this class, use NCGroupCollection.createWedmIntGeomBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
WedmNocoreGeomBuilder
Represents a WedmNocoreGeom Builder
To create a new instance of this class, use NCGroupCollection.createWedmNocoreGeomBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
interface |
WedmOpenGeomBuilder
Represents a WedmOpenGeom Builder
To create a new instance of this class, use NCGroupCollection.createWedmOpenGeomBuilder(nxopen.cam.CAMObject) Created in NX5.0.0 |
Modifier and Type | Method and Description |
---|---|
WedmBasedGeomBuilder |
NCGroupCollection.createWedmBasedGeomBuilder(CAMObject param)
Creates a wire edm based geometry builder
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.