Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnRoughFinishTestCut.MeasuringPositionTypes |
TurnRoughFinishTestCut.MeasuringPositionTypes.AUTOMATIC
Test Cut Measuring Position: Automatic
|
static TurnRoughFinishTestCut.MeasuringPositionTypes |
TurnRoughFinishTestCut.MeasuringPositionTypes.POINT
Test Cut Measuring Position: Point
|
static TurnRoughFinishTestCut.MeasuringPositionTypes |
TurnRoughFinishTestCut.MeasuringPositionTypes.SAME_AS_FIRST_TEST_CUT
Test Cut Measuring Position: Same as First Test Cut
|
Modifier and Type | Method and Description |
---|---|
TurnRoughFinishTestCut.MeasuringPositionTypes |
TurnRoughFinishTestCut.measuringPosition()
Returns the test cut measuring position
License requirements: None. |
static TurnRoughFinishTestCut.MeasuringPositionTypes |
TurnRoughFinishTestCut.MeasuringPositionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnRoughFinishTestCut.MeasuringPositionTypes |
TurnRoughFinishTestCut.MeasuringPositionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnRoughFinishTestCut.MeasuringPositionTypes[] |
TurnRoughFinishTestCut.MeasuringPositionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnRoughFinishTestCut.setMeasuringPosition(TurnRoughFinishTestCut.MeasuringPositionTypes measuringPosition)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.