Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnRoughFinishTestCut.DirectionTypes |
TurnRoughFinishTestCut.DirectionTypes.FORWARD
Test Direction: Forward
|
static TurnRoughFinishTestCut.DirectionTypes |
TurnRoughFinishTestCut.DirectionTypes.REVERSE
Test Direction: Reverse
|
Modifier and Type | Method and Description |
---|---|
TurnRoughFinishTestCut.DirectionTypes |
TurnRoughFinishTestCut.direction()
Returns the test cut direction
License requirements: None. |
static TurnRoughFinishTestCut.DirectionTypes |
TurnRoughFinishTestCut.DirectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnRoughFinishTestCut.DirectionTypes |
TurnRoughFinishTestCut.DirectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnRoughFinishTestCut.DirectionTypes[] |
TurnRoughFinishTestCut.DirectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnRoughFinishTestCut.setDirection(TurnRoughFinishTestCut.DirectionTypes direction)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.