Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnProbeClearanceBuilder.AxialPlaneModes |
TurnProbeClearanceBuilder.AxialPlaneModes.DISTANCE
Plane is defined by distance value.
|
static TurnProbeClearanceBuilder.AxialPlaneModes |
TurnProbeClearanceBuilder.AxialPlaneModes.NONE
Plane is inactive.
|
static TurnProbeClearanceBuilder.AxialPlaneModes |
TurnProbeClearanceBuilder.AxialPlaneModes.POINT
Plane is defined by point.
|
Modifier and Type | Method and Description |
---|---|
TurnProbeClearanceBuilder.AxialPlaneModes |
TurnProbeClearanceBuilder.axialPlaneMode()
Returns the axial plane mode
License requirements: None. |
static TurnProbeClearanceBuilder.AxialPlaneModes |
TurnProbeClearanceBuilder.AxialPlaneModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnProbeClearanceBuilder.AxialPlaneModes |
TurnProbeClearanceBuilder.AxialPlaneModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnProbeClearanceBuilder.AxialPlaneModes[] |
TurnProbeClearanceBuilder.AxialPlaneModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnProbeClearanceBuilder.setAxialPlaneMode(TurnProbeClearanceBuilder.AxialPlaneModes axialPlaneMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.