Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnAvoidanceStartBuilder.StartPointModes |
TurnAvoidanceStartBuilder.StartPointModes.DELTA_ANGLE_DISTANCE
Point is defined by angle and distance.
|
static TurnAvoidanceStartBuilder.StartPointModes |
TurnAvoidanceStartBuilder.StartPointModes.DELTA_MOVE
Point is defined by delta move (X and Y coordinate).
|
static TurnAvoidanceStartBuilder.StartPointModes |
TurnAvoidanceStartBuilder.StartPointModes.DELTA_VECTOR_DISTANCE
Point is defined by vector and distance.
|
static TurnAvoidanceStartBuilder.StartPointModes |
TurnAvoidanceStartBuilder.StartPointModes.POINT
Point is defined by point.
|
Modifier and Type | Method and Description |
---|---|
TurnAvoidanceStartBuilder.StartPointModes |
TurnAvoidanceStartBuilder.startPointMode()
Returns the start point mode
License requirements: None. |
static TurnAvoidanceStartBuilder.StartPointModes |
TurnAvoidanceStartBuilder.StartPointModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceStartBuilder.StartPointModes |
TurnAvoidanceStartBuilder.StartPointModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceStartBuilder.StartPointModes[] |
TurnAvoidanceStartBuilder.StartPointModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnAvoidanceStartBuilder.setStartPointMode(TurnAvoidanceStartBuilder.StartPointModes startPointMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.