Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.AUTOMATIC
Motion type: Automatic to point.
|
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.AXIAL_THEN_RADIAL
Motion type: Axial then axial to point.
|
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.CLEAR_AXIAL_ONLY
Motion type: Axial to clearance plane only (no motion to point).
|
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.CLEAR_AXIAL_THEN_DIRECT
Motion type: Axial to clearance plane then direct to point.
|
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.CLEAR_RADIAL_ONLY
Motion type: Radial to clearance plane only (no motion to point).
|
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.CLEAR_RADIAL_THEN_DIRECT
Motion type: Radial to clearance plane then direct to point.
|
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.DIRECT
Motion type: Direct to point.
|
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.NONE
Point is inactive.
|
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.RADIAL_THEN_AXIAL
Motion type: Radial then axial to point.
|
Modifier and Type | Method and Description |
---|---|
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.returnPointMotionType()
Returns the return point motion type
License requirements: None. |
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceReturnBuilder.ReturnPointMotionTypes[] |
TurnAvoidanceReturnBuilder.ReturnPointMotionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnAvoidanceReturnBuilder.setReturnPointMotionType(TurnAvoidanceReturnBuilder.ReturnPointMotionTypes returnPointMotionType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.