Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnAvoidanceClearanceBuilder.RadialPlaneModes |
TurnAvoidanceClearanceBuilder.RadialPlaneModes.DISTANCE
Plane is defined by distance value.
|
static TurnAvoidanceClearanceBuilder.RadialPlaneModes |
TurnAvoidanceClearanceBuilder.RadialPlaneModes.NONE
Plane is inactive.
|
static TurnAvoidanceClearanceBuilder.RadialPlaneModes |
TurnAvoidanceClearanceBuilder.RadialPlaneModes.POINT
Plane is defined by point.
|
Modifier and Type | Method and Description |
---|---|
TurnAvoidanceClearanceBuilder.RadialPlaneModes |
TurnAvoidanceClearanceBuilder.radialPlaneMode()
Returns the radial plane mode
License requirements: None. |
static TurnAvoidanceClearanceBuilder.RadialPlaneModes |
TurnAvoidanceClearanceBuilder.RadialPlaneModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceClearanceBuilder.RadialPlaneModes |
TurnAvoidanceClearanceBuilder.RadialPlaneModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceClearanceBuilder.RadialPlaneModes[] |
TurnAvoidanceClearanceBuilder.RadialPlaneModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnAvoidanceClearanceBuilder.setRadialPlaneMode(TurnAvoidanceClearanceBuilder.RadialPlaneModes radialPlaneMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.