Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TrimPoint.RampAngleOptions |
TrimPoint.RampAngleOptions.ALIGNED
Ramp angle is aligned to angle.
|
static TrimPoint.RampAngleOptions |
TrimPoint.RampAngleOptions.ANGLE
Ramp angle is defined by a value.
|
static TrimPoint.RampAngleOptions |
TrimPoint.RampAngleOptions.NONE
no ramp angle.
|
static TrimPoint.RampAngleOptions |
TrimPoint.RampAngleOptions.VECTOR
Ramp angle is defined by a vector.
|
Modifier and Type | Method and Description |
---|---|
TrimPoint.RampAngleOptions |
TrimPoint.rampAngleOption()
Returns the trim point ramp angle option
License requirements: None. |
static TrimPoint.RampAngleOptions |
TrimPoint.RampAngleOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimPoint.RampAngleOptions |
TrimPoint.RampAngleOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimPoint.RampAngleOptions[] |
TrimPoint.RampAngleOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimPoint.setRampAngleOption(TrimPoint.RampAngleOptions rampAngleMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.