Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
ToolPathSplitItemBuilder |
ToolPathSplitBuilder.createToolPathSplitItemBuilder()
The method to create the SplitToolPathItemBuilder
License requirements: cam_base ("CAM BASE") . |
ToolPathSplitItemBuilder |
ToolPathSplitItemBuilderList.findItem(int index)
Returns the object at the input index.
|
ToolPathSplitItemBuilder[] |
ToolPathSplitItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ToolPathSplitItemBuilderList.append(ToolPathSplitItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
ToolPathSplitItemBuilderList.append(ToolPathSplitItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ToolPathSplitItemBuilderList.erase(ToolPathSplitItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ToolPathSplitItemBuilderList.erase(ToolPathSplitItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ToolPathSplitItemBuilderList.findIndex(ToolPathSplitItemBuilder obj)
Finds the index where the input object appears.
|
void |
ToolPathSplitItemBuilderList.insert(int location,
ToolPathSplitItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ToolPathSplitItemBuilderList.setContents(ToolPathSplitItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
ToolPathSplitItemBuilderList.swap(ToolPathSplitItemBuilder object1,
ToolPathSplitItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.