Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static ToolAxisInterpolate.ControlDirectionTypes |
ToolAxisInterpolate.ControlDirectionTypes.U
U only
|
static ToolAxisInterpolate.ControlDirectionTypes |
ToolAxisInterpolate.ControlDirectionTypes.UANDV
U and V
|
static ToolAxisInterpolate.ControlDirectionTypes |
ToolAxisInterpolate.ControlDirectionTypes.V
V only
|
Modifier and Type | Method and Description |
---|---|
ToolAxisInterpolate.ControlDirectionTypes |
ToolAxisInterpolate.controlDirection()
Returns the control direction type
License requirements: None. |
static ToolAxisInterpolate.ControlDirectionTypes |
ToolAxisInterpolate.ControlDirectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ToolAxisInterpolate.ControlDirectionTypes |
ToolAxisInterpolate.ControlDirectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ToolAxisInterpolate.ControlDirectionTypes[] |
ToolAxisInterpolate.ControlDirectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ToolAxisInterpolate.setControlDirection(ToolAxisInterpolate.ControlDirectionTypes newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.