Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TeachmodeLinearMoveBuilder.MoveTypes |
TeachmodeLinearMoveBuilder.MoveTypes.AXIAL
Axial only
|
static TeachmodeLinearMoveBuilder.MoveTypes |
TeachmodeLinearMoveBuilder.MoveTypes.AXIAL_RADIAL
Axial then Radial
|
static TeachmodeLinearMoveBuilder.MoveTypes |
TeachmodeLinearMoveBuilder.MoveTypes.DIRECT
Direct
|
static TeachmodeLinearMoveBuilder.MoveTypes |
TeachmodeLinearMoveBuilder.MoveTypes.RADIAL
Radial only
|
static TeachmodeLinearMoveBuilder.MoveTypes |
TeachmodeLinearMoveBuilder.MoveTypes.RADIAL_AXIAL
Radial then Axial
|
Modifier and Type | Method and Description |
---|---|
TeachmodeLinearMoveBuilder.MoveTypes |
TeachmodeLinearMoveBuilder.moveType()
Returns the Movement Type
License requirements: None. |
static TeachmodeLinearMoveBuilder.MoveTypes |
TeachmodeLinearMoveBuilder.MoveTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TeachmodeLinearMoveBuilder.MoveTypes |
TeachmodeLinearMoveBuilder.MoveTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TeachmodeLinearMoveBuilder.MoveTypes[] |
TeachmodeLinearMoveBuilder.MoveTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TeachmodeLinearMoveBuilder.setMoveType(TeachmodeLinearMoveBuilder.MoveTypes newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.