Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static SurfaceContourBuilder.AccessVectorMethodType |
SurfaceContourBuilder.AccessVectorMethodType.AWAY_FROM_LINE
away from the vector defined
|
static SurfaceContourBuilder.AccessVectorMethodType |
SurfaceContourBuilder.AccessVectorMethodType.NEG_ZM
negative z-direction of MCS
|
static SurfaceContourBuilder.AccessVectorMethodType |
SurfaceContourBuilder.AccessVectorMethodType.SPECIFY
user specified
|
static SurfaceContourBuilder.AccessVectorMethodType |
SurfaceContourBuilder.AccessVectorMethodType.TOWARD_LINE
toward the vector defined
|
static SurfaceContourBuilder.AccessVectorMethodType |
SurfaceContourBuilder.AccessVectorMethodType.ZM
positive z-direction of MCS
|
Modifier and Type | Method and Description |
---|---|
SurfaceContourBuilder.AccessVectorMethodType |
SurfaceContourBuilder.accessVectorMethod()
Returns the Access Vector Method
License requirements: None. |
static SurfaceContourBuilder.AccessVectorMethodType |
SurfaceContourBuilder.AccessVectorMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SurfaceContourBuilder.AccessVectorMethodType |
SurfaceContourBuilder.AccessVectorMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SurfaceContourBuilder.AccessVectorMethodType[] |
SurfaceContourBuilder.AccessVectorMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SurfaceContourBuilder.setAccessVectorMethod(SurfaceContourBuilder.AccessVectorMethodType accessVectorMethod)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.