Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
Splitter |
MultiBladeSplittersGeometry.createSplitter(NXObject[] wallFaces,
NXObject[] blendFaces)
Create a new splitter
License requirements: cam_base ("CAM BASE") . |
Splitter |
SplitterList.findItem(int index)
Returns the object at the input index.
|
Splitter[] |
SplitterList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SplitterList.append(Splitter object)
Appends an object to the list
License requirements: None. |
void |
SplitterList.append(Splitter[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SplitterList.erase(Splitter obj)
Erases the object from the list, but does not delete the object.
|
void |
SplitterList.erase(Splitter obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SplitterList.findIndex(Splitter obj)
Finds the index where the input object appears.
|
void |
SplitterList.insert(int location,
Splitter object)
Inserts an object at the specified location
License requirements: None. |
void |
SplitterList.setContents(Splitter[] objects)
Sets the contents of the entire list.
|
void |
SplitterList.swap(Splitter object1,
Splitter object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.