Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static SimulationOptionsBuilder.Resolution |
SimulationOptionsBuilder.Resolution.EXTRA_FINE
use extra fine resolution
|
static SimulationOptionsBuilder.Resolution |
SimulationOptionsBuilder.Resolution.FAST
use fast resolution
|
static SimulationOptionsBuilder.Resolution |
SimulationOptionsBuilder.Resolution.FINE
use fine resolution
|
static SimulationOptionsBuilder.Resolution |
SimulationOptionsBuilder.Resolution.NORMAL
use normal resolution
|
Modifier and Type | Method and Description |
---|---|
SimulationOptionsBuilder.Resolution |
SimulationOptionsBuilder.ipwResolution()
Returns the ipw resolution
License requirements: None. |
static SimulationOptionsBuilder.Resolution |
SimulationOptionsBuilder.Resolution.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimulationOptionsBuilder.Resolution |
SimulationOptionsBuilder.Resolution.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimulationOptionsBuilder.Resolution[] |
SimulationOptionsBuilder.Resolution.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SimulationOptionsBuilder.setIpwResolution(SimulationOptionsBuilder.Resolution ipwResolution)
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.