Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static PitchSetting.OptionTypes |
PitchSetting.OptionTypes.LEAD
Lead
|
static PitchSetting.OptionTypes |
PitchSetting.OptionTypes.PITCH
Pitch
|
static PitchSetting.OptionTypes |
PitchSetting.OptionTypes.THREADS_PER_UNIT
Threads per mm or inch
|
Modifier and Type | Method and Description |
---|---|
PitchSetting.OptionTypes |
PitchSetting.option()
Returns the pitch option
License requirements: None. |
static PitchSetting.OptionTypes |
PitchSetting.OptionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PitchSetting.OptionTypes |
PitchSetting.OptionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PitchSetting.OptionTypes[] |
PitchSetting.OptionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PitchSetting.setOption(PitchSetting.OptionTypes pitchOption)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.