Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static OrientGeomBuilder.SpecialOutputModes |
OrientGeomBuilder.SpecialOutputModes.CSYS_ROTATION
Special output mode: CSYS rotation
|
static OrientGeomBuilder.SpecialOutputModes |
OrientGeomBuilder.SpecialOutputModes.FIXTURE_OFFSET
Special output mode: Fixture offset
|
static OrientGeomBuilder.SpecialOutputModes |
OrientGeomBuilder.SpecialOutputModes.NONE
Special output mode: None
|
static OrientGeomBuilder.SpecialOutputModes |
OrientGeomBuilder.SpecialOutputModes.USE_MAIN_MCS
Special output mode: Use main MCS
|
Modifier and Type | Method and Description |
---|---|
OrientGeomBuilder.SpecialOutputModes |
OrientGeomBuilder.getSpecialOutputMode()
Returns the Special Output
License requirements: cam_base ("CAM BASE") . |
static OrientGeomBuilder.SpecialOutputModes |
OrientGeomBuilder.SpecialOutputModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientGeomBuilder.SpecialOutputModes |
OrientGeomBuilder.SpecialOutputModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientGeomBuilder.SpecialOutputModes[] |
OrientGeomBuilder.SpecialOutputModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientGeomBuilder.setSpecialOutputMode(OrientGeomBuilder.SpecialOutputModes specialOutputMode)
Sets the Special Output
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.