Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static OperationTransformBuilder.Angle |
OperationTransformBuilder.Angle.SPECIFY
specify a angle
|
static OperationTransformBuilder.Angle |
OperationTransformBuilder.Angle.TWO_POINT
use two point to sepcify a angle
|
Modifier and Type | Method and Description |
---|---|
OperationTransformBuilder.Angle |
OperationTransformBuilder.angleMethod()
Returns the angle method
License requirements: None. |
static OperationTransformBuilder.Angle |
OperationTransformBuilder.Angle.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OperationTransformBuilder.Angle |
OperationTransformBuilder.Angle.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OperationTransformBuilder.Angle[] |
OperationTransformBuilder.Angle.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OperationTransformBuilder.setAngleMethod(OperationTransformBuilder.Angle angleMethod)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.