Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static OperationDisplayOptionsBuilder.PathNormalTypes |
OperationDisplayOptionsBuilder.PathNormalTypes.TYPES_SPECIFY
Path Normal: Specify
|
static OperationDisplayOptionsBuilder.PathNormalTypes |
OperationDisplayOptionsBuilder.PathNormalTypes.TYPES_TOOL_AXIS
Path Normal: Tool axis
|
Modifier and Type | Method and Description |
---|---|
OperationDisplayOptionsBuilder.PathNormalTypes |
OperationDisplayOptionsBuilder.pathNormalType()
Returns the path normal types
License requirements: None. |
static OperationDisplayOptionsBuilder.PathNormalTypes |
OperationDisplayOptionsBuilder.PathNormalTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OperationDisplayOptionsBuilder.PathNormalTypes |
OperationDisplayOptionsBuilder.PathNormalTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OperationDisplayOptionsBuilder.PathNormalTypes[] |
OperationDisplayOptionsBuilder.PathNormalTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OperationDisplayOptionsBuilder.setPathNormalType(OperationDisplayOptionsBuilder.PathNormalTypes pathNormal)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.